What kind of license (Basic, Standard or Professional) I need purchase for Kinetis MCUs?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What kind of license (Basic, Standard or Professional) I need purchase for Kinetis MCUs?

跳至解决方案
3,175 次查看
Magnetron
Contributor III

What kind of license (Basic, Standard or Professional) I need purchase in order to get available all features (unlimited) for developing for Kinetis MCUs only?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,424 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Magnetron,

you may visit the Features link and click on the Kinetis section, it will give you all the features that are inclded in all the CodeWarrior suite.  Or you may click on the home link and use the selector to get the best option for you.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,425 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Magnetron,

you may visit the Features link and click on the Kinetis section, it will give you all the features that are inclded in all the CodeWarrior suite.  Or you may click on the home link and use the selector to get the best option for you.

0 项奖励
回复
2,424 次查看
Magnetron
Contributor III

Anybody form Freescale Sale department can fill last line of the attached table (and win $1 :-))?

0 项奖励
回复
2,424 次查看
CrasyCat
Specialist III

Hello

 

I have checked with product management and indicated we are missing Kinetis specific information for the various editions.

 

Basically, special edition comes with a size limitation of 128 K. Meaning you can build ANSI C application with up to 128 K of code and data.

 

Standard edition allows to develop ANSI C application without any limitation in size ANSI C source code.

 

Professional edition allows you to develop ANSI C & C++ application without any size limitation.

 

Note that if you are using MQX OS, only the professional edition comes with support for MQX kernel awareness in the debugger.

 

I hope this helps.

 

 

CrasyCat

0 项奖励
回复
2,424 次查看
Magnetron
Contributor III

Thx.

0 项奖励
回复