What kind of license (Basic, Standard or Professional) I need purchase for Kinetis MCUs?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What kind of license (Basic, Standard or Professional) I need purchase for Kinetis MCUs?

Jump to solution
3,127 Views
Magnetron
Contributor III

What kind of license (Basic, Standard or Professional) I need purchase in order to get available all features (unlimited) for developing for Kinetis MCUs only?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,376 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Magnetron,

you may visit the Features link and click on the Kinetis section, it will give you all the features that are inclded in all the CodeWarrior suite.  Or you may click on the home link and use the selector to get the best option for you.

View solution in original post

0 Kudos
Reply
4 Replies
2,377 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Magnetron,

you may visit the Features link and click on the Kinetis section, it will give you all the features that are inclded in all the CodeWarrior suite.  Or you may click on the home link and use the selector to get the best option for you.

0 Kudos
Reply
2,376 Views
Magnetron
Contributor III

Anybody form Freescale Sale department can fill last line of the attached table (and win $1 :-))?

0 Kudos
Reply
2,376 Views
CrasyCat
Specialist III

Hello

 

I have checked with product management and indicated we are missing Kinetis specific information for the various editions.

 

Basically, special edition comes with a size limitation of 128 K. Meaning you can build ANSI C application with up to 128 K of code and data.

 

Standard edition allows to develop ANSI C application without any limitation in size ANSI C source code.

 

Professional edition allows you to develop ANSI C & C++ application without any size limitation.

 

Note that if you are using MQX OS, only the professional edition comes with support for MQX kernel awareness in the debugger.

 

I hope this helps.

 

 

CrasyCat

0 Kudos
Reply
2,376 Views
Magnetron
Contributor III

Thx.

0 Kudos
Reply