30-day evaluation license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

30-day evaluation license

ソリューションへジャンプ
6,070件の閲覧回数
Smay
Contributor I
Hello,
I downloaded an evaluation copy of Codewarrior HC12 V4.6 to test it with a MC9S12NE64 microprocessor. I would like to obtain a 30-day evaluation license and sent a mail to license@freescale.com as discribed in the download menu. Unfortunately I haven´t received a response yet :smileysad:
 
Do I have to send some special information (i.e. about the project) or did something else wrong?
 
Thanks,
Stefan May
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,383件の閲覧回数
Alban
Senior Contributor II
Hello Wayne,
 
Add this line in your license.dat file:
 
Code:
FEATURE PE_Advanced_BeansHCS12 metrowks 1.000 1-apr-2007 uncounted \ 253ADD6B8B01 VENDOR_STRING=163E94D42D01E5E171C0105CC88049C5 \ HOSTID=ANY ck=97

 
Expiration date is 1st April = 1 month.
 
Alban.

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
3,383件の閲覧回数
WayneHowell
Contributor I
Hello,
 
I'm going mad fighting with license files. Anyone please help!
 
After much pain I know have V4.6 Codewarrior prof version installed. I have a 30 day license installed which has removed the file number and code size limit.
 
The problem is that I'm using advanced beans in the processor expert (Ethernet). When I compile, an error message informs me my license does not allow advanced beans.
 
But tech support in the UK and the freescale web site confirm that the 30 day prof license should allow this.
 
Help .....
 
Wayne Howell
0 件の賞賛
返信
3,383件の閲覧回数
Smay
Contributor I
Got the license file today.
Thanks alot :smileyhappy:
 
Stefan May
0 件の賞賛
返信
3,383件の閲覧回数
Alban
Senior Contributor II
Hello Wayne,
 
When updating the license.dat, I always append the information and not remove the previous content.
If you could indicate the ERROR Code that could help us giving you the right line for the license.
 
Cheers,
Alban.
0 件の賞賛
返信
3,383件の閲覧回数
WayneHowell
Contributor I
Hi there,
 
The error is displayed when I load the project. Code is -5,357. Message "Processor Expertlicense 'Advanced Beans' for HCS12 family was not found or is not valid".
 
Flexlm detailed info:
 
No such feature exists.
Feature PE_Advanced_BeansHCS12
 
 
Hope you can help.
 
Thanks
 
Wayne
0 件の賞賛
返信
3,383件の閲覧回数
WayneHowell
Contributor I
Hi,
 
More info:
 
The Bean wizard also causes the same error code and then locks up Code Warrior.
 
Thanks
 
Wayne
0 件の賞賛
返信
3,384件の閲覧回数
Alban
Senior Contributor II
Hello Wayne,
 
Add this line in your license.dat file:
 
Code:
FEATURE PE_Advanced_BeansHCS12 metrowks 1.000 1-apr-2007 uncounted \ 253ADD6B8B01 VENDOR_STRING=163E94D42D01E5E171C0105CC88049C5 \ HOSTID=ANY ck=97

 
Expiration date is 1st April = 1 month.
 
Alban.
0 件の賞賛
返信
3,383件の閲覧回数
WayneHowell
Contributor I
Hi Alban,
 
Many thanks that has got the advanced bean working.
 
Unfortunately the Bean Wizard is still not working, although it no longer crashes.
 
The error code is: -5,357.
 
Thanks.
 
Wayne
0 件の賞賛
返信
3,383件の閲覧回数
Alban
Senior Contributor II
Hello,
 
Please send me your email address via Private Message so we can fix that. Not on the board.
 
Cheers,
Alban.
0 件の賞賛
返信
3,382件の閲覧回数
WayneHowell
Contributor I
0 件の賞賛
返信
3,382件の閲覧回数
Alban
Senior Contributor II
Hello Stefan
 
I believe the information you are looking for is in the link:
 
Cheers,
Alban.
0 件の賞賛
返信