HI NXP team,
for TPMS RF application we are using NXP NTM88 ic as a transmitter where as NXP lizard V2 board as a receiver,
in attached image i have a question
1) i was changed payload length 18 in a code but it still show 12, why? or that 12 has another meaning in the CDK tool
2) the z Coolum having a data 80 and C0 what is that? and what is an write value 80 or C0?
please help me out from it
tanks and regards,
Pranav Tonape
Hello Pranav,
1. Is data in column H displayed in hexa or decimal? Because 0x12 = 18. So, if data is displayed in hexa, it corresponds to a payload length of 18 bytes.
2. These are code violation bits. They are explained in the AN13717.
BR, Tomas