mc33771

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc33771

4,230 Views
jaures168
Contributor II

我們目前在SPEC還無法得知的如下圖部分, 對於Cell voltage Max/Min error value?

about mc33771 that Cell voltage Max/Min error value?

i want know -40c~125c full temp range?

please gibe us the Verr ~VERR5 that min/max at  -40c~125c

our customer want to know which range.

do you test report at mc33771?

see attached pdf 

MC33771B_SDS

Battery cell controller IC

Rev. 5.0 2 May 2018 Short data sheet: technical data

page 13/29

asap tell me

mc33771jpg.jpg

0 Kudos
Reply
4 Replies

2,178 Views
lisettelozano
NXP Employee
NXP Employee

Hello Jaures,

Please see the complete values below:

pastedImage_1.png

If you want a complete datasheet, please create a standard ticket to request it. 

Have a great day,

Paulina

0 Kudos
Reply

2,178 Views
jaures168
Contributor II

hi Paulina

Which ones are temperature offset, which are constant errors!

if constant errors than us use software calibration.

and do you detail test report ? 

we want to detail review the report.

may we can save the error!

0 Kudos
Reply

2,178 Views
lisettelozano
NXP Employee
NXP Employee

Hi Jaures,

The values showed in the image are constants errors for the temperature and voltage range mentioned on each one of them.

In regards to the test report, unfortunately, we do not have that document or information to provide. I apologize for the inconvenience that this may cause.

Have a great day, 

Paulina

0 Kudos
Reply

2,178 Views
jaures168
Contributor II

hi Paulina

i want to use  mc33771 14 pcs  series to 196 cell,but how to initial 

about the transformer daisy chain the cluster 1~15 :

how to use software to set the cluster 1~15?

Use Device Address (Cluster ID) 0~15 to setting daisy chain the cluster 1~15.

but how to initial the Device Address (Cluster ID) 0~15.?

do you app note to me,or tell me how to use software to set  mc33771 14 pcs?

asap

mc33771daisychain.jpg

mc33771CID.jpg

0 Kudos
Reply