mMPXV7002DP Airspeed measurement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mMPXV7002DP Airspeed measurement

Jump to solution
1,064 Views
nadi_abumahfouz
Contributor I

Hello,

I'm using mMPXV7002DP and I'm trying to convert the output to measure airspeed. knowing the output pin connected to ADC with 3.3V refrence. how can I convert the output value to measure airspeed? 

Thanks,

Nadi

Labels (1)
1 Solution
944 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Nadi,

First off, have a look at Dynamic pressure - Wikipedia.

Dynamic pressure = 0.5 x density x velocity x velocity
You can use 1.225kg/m3 for sea level air density. Velocity should be m/s. Pressure will be in Pascals.

Then you need to know how many Pascals correspond to 1 ADC count. 

For example, if you have an 8-bit ADC with a 3.3V reference and considering typical sensitivity of 1V/kPa , then 1 ADC count corresponds to 12.89Pa.

Hope it helps.

Best regards,

Tomas

View solution in original post

2 Replies
945 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Nadi,

First off, have a look at Dynamic pressure - Wikipedia.

Dynamic pressure = 0.5 x density x velocity x velocity
You can use 1.225kg/m3 for sea level air density. Velocity should be m/s. Pressure will be in Pascals.

Then you need to know how many Pascals correspond to 1 ADC count. 

For example, if you have an 8-bit ADC with a 3.3V reference and considering typical sensitivity of 1V/kPa , then 1 ADC count corresponds to 12.89Pa.

Hope it helps.

Best regards,

Tomas

944 Views
nadi_abumahfouz
Contributor I

Thank you Tomas, this is really helpful I understand everything right now.

Thanks,

Nadi

0 Kudos
Reply