fxls90322加速度传感器spi发送命了响应数据和预期值不一致

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fxls90322加速度传感器spi发送命了响应数据和预期值不一致

Jump to solution
402 Views
shanY1
Contributor I

异常响应值异常响应值

 

根据spi编程建议的命令 0x8010012A的预期值是0x00000000实际抓取到的值是0x40100033

0 Kudos
Reply
1 Solution
374 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Yakai,

please refer to the Figure 4. in the AN12386. The response to the 0x8010012A doesn't have to be 0x00000000, because the FXLS90322 is in reset and is not driving the MISO pin. 

JozefKozon_0-1705300998477.png

So even the 0x40100033 can be correct. 

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
1 Reply
375 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Yakai,

please refer to the Figure 4. in the AN12386. The response to the 0x8010012A doesn't have to be 0x00000000, because the FXLS90322 is in reset and is not driving the MISO pin. 

JozefKozon_0-1705300998477.png

So even the 0x40100033 can be correct. 

With Best Regards,

Jozef

0 Kudos
Reply