fxls90322加速度传感器spi发送命了响应数据和预期值不一致

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

fxls90322加速度传感器spi发送命了响应数据和预期值不一致

跳至解决方案
326 次查看
shanY1
Contributor I

异常响应值异常响应值

 

根据spi编程建议的命令 0x8010012A的预期值是0x00000000实际抓取到的值是0x40100033

0 项奖励
回复
1 解答
298 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Yakai,

please refer to the Figure 4. in the AN12386. The response to the 0x8010012A doesn't have to be 0x00000000, because the FXLS90322 is in reset and is not driving the MISO pin. 

JozefKozon_0-1705300998477.png

So even the 0x40100033 can be correct. 

With Best Regards,

Jozef

在原帖中查看解决方案

0 项奖励
回复
1 回复
299 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Yakai,

please refer to the Figure 4. in the AN12386. The response to the 0x8010012A doesn't have to be 0x00000000, because the FXLS90322 is in reset and is not driving the MISO pin. 

JozefKozon_0-1705300998477.png

So even the 0x40100033 can be correct. 

With Best Regards,

Jozef

0 项奖励
回复