fxls90322加速度传感器spi发送命了响应数据和预期值不一致

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fxls90322加速度传感器spi发送命了响应数据和预期值不一致

ソリューションへジャンプ
401件の閲覧回数
shanY1
Contributor I

异常响应值异常响应值

 

根据spi编程建议的命令 0x8010012A的预期值是0x00000000实际抓取到的值是0x40100033

0 件の賞賛
返信
1 解決策
373件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Yakai,

please refer to the Figure 4. in the AN12386. The response to the 0x8010012A doesn't have to be 0x00000000, because the FXLS90322 is in reset and is not driving the MISO pin. 

JozefKozon_0-1705300998477.png

So even the 0x40100033 can be correct. 

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
374件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Yakai,

please refer to the Figure 4. in the AN12386. The response to the 0x8010012A doesn't have to be 0x00000000, because the FXLS90322 is in reset and is not driving the MISO pin. 

JozefKozon_0-1705300998477.png

So even the 0x40100033 can be correct. 

With Best Regards,

Jozef

0 件の賞賛
返信