I am using NTM88 dual axis sensor for TPMS application,NTM88 is being used as transmitter and NCK2910 EVK as receiver. I have installed the sensor on Wheel rim of a vehicle and distance between sensor and receiver is 14ft to 16ft, output power of sensor is 8dBm . RF data packets are received properly at the receivers end when sensor is stationary or wheel is not rotating, but as soon as i start rotating the wheel above @20Kmph packets start missing or corrupted.
Is there a way to avoid or minimize the missing packets?
Solved! Go to Solution.
Hello Ankit,
The following strategies can be used to improve the reception rate:
BR, Tomas
Hello Ankit,
The following strategies can be used to improve the reception rate:
BR, Tomas
Hello Ankit,
Yes, sending the packet at a particular angle may reduce the packet losses. Depending on the position of the receiver in the car, there may be a transmission path that would optimize the reception rate.
However, running the angle location algorithm consumes power. So, it is necessary to compare the consumption and reception rate of both solutions (using transmission randomization and using angle location) to determine which one is most appropriate.
BR, Tomas