Hello, I have a question about the error in the datasheet.
Data Sheet Freescale: MPXV7002 Rev 2, 1/2009, Page 2
Pressure Offset(3) (10 to 60°C) @ VS = 5.0 Volts Voff 2.25 2.5 2.75 Vdc
and
Data Sheet NXP: Document Number: MPXV7002, Rev 4, 03/2017, Page 3
Pressure Offset(3) (10 to 60°C) @ VS = 5.0 Volts Voff 0.25 0.5 0.75 Vdc
Please let me know if you have a mistake in your datasheet (MPXV7002, Rev 4, 03/2017) at Pressure Offset Max=0,75Vdc.
The original from Freescale was worth Max=2,75Vdc.
Thank you in advance.
Best Ragards
Milos Kovacik
Hi Milos,
As the offset is defined as the output voltage at the minimum rated pressure which is -2 kPa, the correct values (min. 0.25V, typ. 0.5V, max. 0.75V) are shown in the latest NXP Data Sheet Rev 4.
However, with no pressure difference between P1 and P2, the output voltage will be around 2.5V (min. 2.25V, max. 2.75V).
Best regards,
Tomas