MPXV7002: -2 to 2kPa, Vacuum Pressure Sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXV7002: -2 to 2kPa, Vacuum Pressure Sensor

577 Views
info14
Contributor I

Hello, I have a question about the error in the datasheet.

Data Sheet Freescale: MPXV7002 Rev 2, 1/2009, Page 2

Pressure Offset(3) (10 to 60°C) @ VS = 5.0 Volts  Voff 2.25 2.5 2.75 Vdc

and

Data Sheet NXP: Document Number: MPXV7002, Rev 4, 03/2017, Page 3

Pressure Offset(3) (10 to 60°C) @ VS = 5.0 Volts  Voff 0.25 0.5 0.75 Vdc

Please let me know if you have a mistake in your datasheet (MPXV7002, Rev 4, 03/2017) at Pressure Offset Max=0,75Vdc.

The original from Freescale was worth Max=2,75Vdc.

Thank you in advance.

Best Ragards

Milos Kovacik

Labels (1)
0 Kudos
1 Reply

488 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Milos,

As the offset is defined as the output voltage at the minimum rated pressure which is -2 kPa, the correct values (min. 0.25V, typ. 0.5V, max. 0.75V) are shown in the latest NXP Data Sheet Rev 4. 

However, with no pressure difference between P1 and P2, the output voltage will be around 2.5V (min. 2.25V, max. 2.75V).

Best regards,

Tomas

0 Kudos