MPXV5010G PIN CONFIGURATION

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPXV5010G PIN CONFIGURATION

564件の閲覧回数
kumod
Contributor II

mpxv5010g WITH PORT SENSOR , WHAT IS PIN NUMBERS OF Vsup, Vout, GND ; 2,4,3 .. this sensor is not working for vaccume pressure results are for 0 kpa shows 0.19volt and for 40kpa shows 0.038volt output please support 

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

462件の閲覧回数
kumod
Contributor II

what will happen if p2 port will sealed ?

0 件の賞賛
返信

547件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The pin assignment is as follows:

1 – N/C

2 – Vs (Supply Voltage)

3 – GND (Ground)

4 – Vout (Output Voltage)

5 – N/C

6 – N/C

7 – N/C

8 – N/C

Pin 1 can be identified by a small notch in the lead.

Please note that the MPXV5010G is a gauge pressure sensor measuring the pressure difference between the P1 port (input pressure) and an ambient pressure. 

If you are looking for a vacuum pressure sensor, I would recommend you the MPXV5050V.

BR, Tomas

0 件の賞賛
返信

537件の閲覧回数
kumod
Contributor II

Thanks for reply,

  first i have used MPXV10gc but which was uncompensated , then i have tried mpx5010 , please suggest the signal conditioning for MPXV10gc with actual component values i have used AN but not understood properly to design system  

0 件の賞賛
返信