mpxv5010g WITH PORT SENSOR , WHAT IS PIN NUMBERS OF Vsup, Vout, GND ; 2,4,3 .. this sensor is not working for vaccume pressure results are for 0 kpa shows 0.19volt and for 40kpa shows 0.038volt output please support
what will happen if p2 port will sealed ?
Hi,
The pin assignment is as follows:
1 – N/C
2 – Vs (Supply Voltage)
3 – GND (Ground)
4 – Vout (Output Voltage)
5 – N/C
6 – N/C
7 – N/C
8 – N/C
Pin 1 can be identified by a small notch in the lead.
Please note that the MPXV5010G is a gauge pressure sensor measuring the pressure difference between the P1 port (input pressure) and an ambient pressure.
If you are looking for a vacuum pressure sensor, I would recommend you the MPXV5050V.
BR, Tomas
Thanks for reply,
first i have used MPXV10gc but which was uncompensated , then i have tried mpx5010 , please suggest the signal conditioning for MPXV10gc with actual component values i have used AN but not understood properly to design system