MPXV5010G PIN CONFIGURATION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXV5010G PIN CONFIGURATION

526 Views
kumod
Contributor II

mpxv5010g WITH PORT SENSOR , WHAT IS PIN NUMBERS OF Vsup, Vout, GND ; 2,4,3 .. this sensor is not working for vaccume pressure results are for 0 kpa shows 0.19volt and for 40kpa shows 0.038volt output please support 

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

424 Views
kumod
Contributor II

what will happen if p2 port will sealed ?

0 Kudos
Reply

509 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The pin assignment is as follows:

1 – N/C

2 – Vs (Supply Voltage)

3 – GND (Ground)

4 – Vout (Output Voltage)

5 – N/C

6 – N/C

7 – N/C

8 – N/C

Pin 1 can be identified by a small notch in the lead.

Please note that the MPXV5010G is a gauge pressure sensor measuring the pressure difference between the P1 port (input pressure) and an ambient pressure. 

If you are looking for a vacuum pressure sensor, I would recommend you the MPXV5050V.

BR, Tomas

0 Kudos
Reply

499 Views
kumod
Contributor II

Thanks for reply,

  first i have used MPXV10gc but which was uncompensated , then i have tried mpx5010 , please suggest the signal conditioning for MPXV10gc with actual component values i have used AN but not understood properly to design system  

0 Kudos
Reply