Thank you very much! It need speed sensor or analyze CAN message(speed) from can CAN bus!
Thank you very much! It need speed sensor or analyze CAN message(speed) from can CAN bus!
Dear Jooph,
I am not sure I understand the question, could you or your customer provide more information? What speed are they referring to?
An internal single-axis accelerometer can be used to determine whether a vehicle is moving or stopped, it is not used to calculate the speed based on acceleration data.
Also note that the NTM88H0x5 is a direct TPMS using the pressure transducer to measure the pressure inside the tire. There are also indirect TPMS which typically use the wheel speed sensor.
Best regards,
Tomas