How does the NTM88/PTM88 judge speed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How does the NTM88/PTM88 judge speed?

Jump to solution
1,342 Views
joophliu
Contributor III

Dear NXP Supports:

     How does the NTM88 judge speed?

微信截图_20210111114826.png

   

 

 

Labels (1)
0 Kudos
Reply
1 Solution
1,313 Views
joophliu
Contributor III

Thank you very much! It need speed sensor or analyze CAN message(speed) from can CAN bus!

View solution in original post

0 Kudos
Reply
2 Replies
1,314 Views
joophliu
Contributor III

Thank you very much! It need speed sensor or analyze CAN message(speed) from can CAN bus!

0 Kudos
Reply
1,334 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Jooph,

 

I am not sure I understand the question, could you or your customer provide more information? What speed are they referring to? 

An internal single-axis accelerometer can be used to determine whether a vehicle is moving or stopped, it is not used to calculate the speed based on acceleration data.

Also note that the NTM88H0x5 is a direct TPMS using the pressure transducer to measure the pressure inside the tire. There are also indirect TPMS which typically use the wheel speed sensor.

 

Best regards,

Tomas

0 Kudos
Reply