I want pressure sensor IC whose pressure range is 150kpa to 300 kpa. Please suggest me soon
 
					
				
		
 reyes
		
			reyes
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi prasad bangar,
You can use one of the MPXH6300A Series Family Pressure Sensors: http://cache.freescale.com/files/sensors/doc/data_sheet/MPXH6300A.pdf
The MPXH6300A is an integrated pressure sensor, which means that is On-Chip conditioned and temperature compensated and calibrated and already amplified, which means that you will get an analog output from de sensor from 0 to 4.9V.
For your case, measuring pressure from 150 to 300kPa, you will get an output from about 2.2V (equal to about 150kPa) to 4.9V (about 300kPa).
Please let me know if this pressure sensor works for your application, if not, I can help you to find the correct pressure sensor.
As additional information, we have published a document guide in our communities that can help you to find the correct pressure sensor for your application, you can find this document in the following link: https://community.freescale.com/docs/DOC-102515
Have a great day,
Jose Reyes
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I have read the datasheet mailed by you please send me the details for
purchase of MPXH6300A and whether the IC is available in india with
pricing. Please send me the address in India.
I require it for tyre pressure measurement along with temperature suggest
me your advice whether it is compatible for the given application.
On Mon, Feb 16, 2015 at 11:01 PM, Jose Alberto Reyes Morales <
 
					
				
		
 reyes
		
			reyes
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Peter,
Yes, I think that you can use the MPXH6300A for tyre pressure monitoring.
You can find the details of purchase and availability on our Distribution Network
Have a great day,
Jose Reyes
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------