QFN32 pin terminal open/short test results

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QFN32 pin terminal open/short test results

ソリューションへジャンプ
564件の閲覧回数
hiroyuki_murako
Contributor I

Hello, I am using the S32K116 QFN32 pin.

Could you please give me the test results of the open/short test of the terminal of the QFN32 pin?

Potential Failure Mode
 Pin Open
 Pin Shorted to Ground
 Pin Shorted to adjacent pin (N+1)
 Pin Shorted to Vdd (5V)

S32K116_32qfn

Pin Name

DEFAULT

3

VDD

VDD

4

VSS

VSS

5

PTB7

EXTAL

6

PTB6

XTAL

20

VSS

VSS

21

VDD

VDD

28

PTA10

JTAG_TDO

29

PTC5

JTAG_TDI

30

PTC4

JTAG_TCLK/SWD_CLK

31

PTA5

RESET_b

32

PTA4

JTAG_TMS/SWD_DIO

 

ラベル(1)
タグ(2)
0 件の賞賛
1 解決策
558件の閲覧回数
Yashwant_Singh
NXP Employee
NXP Employee

Hi Hiroyuki,

1. The JTAG and Reset pins are not modelled explicitly in the FMEDA. 

2. The VDD and VSS pins are modelled in the FMEDA and their Failure modes can be seen in the static version under the name of "Package Contacts"

3. NXP's assumed safety concept recommends not to use XOSC as the system clock source and instead use FIRC. (see the attached Safety Manual Snippet). Therefore the XOSC (and hence its package contacts) are marked NSR in the FMEDA and so not reflected in the Static version of the Clock FMEDA. 

Yashwant_Singh_0-1689000513995.png

 

Hope this helps!

Thanks!

-Yashwant.

 

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
559件の閲覧回数
Yashwant_Singh
NXP Employee
NXP Employee

Hi Hiroyuki,

1. The JTAG and Reset pins are not modelled explicitly in the FMEDA. 

2. The VDD and VSS pins are modelled in the FMEDA and their Failure modes can be seen in the static version under the name of "Package Contacts"

3. NXP's assumed safety concept recommends not to use XOSC as the system clock source and instead use FIRC. (see the attached Safety Manual Snippet). Therefore the XOSC (and hence its package contacts) are marked NSR in the FMEDA and so not reflected in the Static version of the Clock FMEDA. 

Yashwant_Singh_0-1689000513995.png

 

Hope this helps!

Thanks!

-Yashwant.

 

0 件の賞賛
555件の閲覧回数
hiroyuki_murako
Contributor I
Dear Yashwant,

Thank you very much for your notice and support.
I was able to understand the content.

Thanks!
0 件の賞賛