Hi,
I installed DS 3.5 AND THE S32K3 DEVELOPMENT PACKAGE AND 3.5.0 RTM DRIVERS AND THERE IS NO EXAMPLE PROJECT ANYWHERE. WHERE WOULD I FIND SOME EXAMPLE PROJECTS?
for k3xx.
Thanks,
Koorosh Hajiani
Hi Peter,
Thank you for your response.
I was able to get the examples. So I imported the project from this path:
C:\NXP\SW32K3_RTD_4.4_2.0.3\eclipse\plugins\Adc_TS_T40D34M20I3R0\examples\S32DS\Adc_example_S32K312,
how ever I can see the function definition and relevant header file are in in the folder one level higher than the example:
C:\NXP\SW32K3_RTD_4.4_2.0.3\eclipse\plugins\Adc_TS_T40D34M20I3R0\source and
C:\NXP\SW32K3_RTD_4.4_2.0.3\eclipse\plugins\Adc_TS_T40D34M20I3R0\include
So my question is how to import this project so that the relevant files from the two folder shown above will be in the project.
Thanks,
Koorosh Hajiani
Hello,
Looks like you will need to set the project paths for correct folders:
Here are the tutorials for S32DS:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-list-of-HOWTOs/ta-p/1113475
best regards,
Peter
Hi,
The link you sent is of absolutely no help. There is nothing on RTD, just SDK.
Anyways I'm closing this case.
Thanks,
Hello,
Not sure about version RTD 3.5.0. but looking at recent available version 4.4.1 - the examples are inside plugins as usual.
Best regards,
Peter