s32k144 Can recover normal staus from bus off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144 Can recover normal staus from bus off

2,630 Views
shingozhou
Contributor III

Hi,

In order to satisfy CAN OSEK network management, I have to recover the CAN normal status from bus-off status in a certain amount of time. And how to configure the CAN registers to meet this requirement?

Obviously, set CAN_CTRL1[BOFFREC] = 1 to disable automatic recovering, because I have to control the time for recovering normal status from bus-off.

I could recall CAN initialzation function to achieve this requirement using other types of MCU, such as STM32. How about S32K144? 

BR

shingo

2 Replies

1,946 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

In case of BOFF_REC = 1 the recovery from bus-off starts after both independent events have become true:

  • 128 occurrences of 11 consecutive recessive bits on the CAN bus have been monitored
  • BOFF_REC has been cleared by the user

So if negation happens

  • before 128 sequences of 11 recessive bits are detected on the CAN bus, then Bus Off recovery happens in similar way as in automatic recovery way.
  • after 128 sequences of 11 recessive bits occurred, then FlexCAN will resynchronize to the bus by waiting for 11 recessive bits before joining the bus.

The CAN init function can be called, depends what is done within it. Obviously SW reset and /or Freeze mode entering is performed together with register setting and MB initialization. So the CAN init could be used for bus-off recover too.

BR, Petr

1,946 Views
shingozhou
Contributor III

Petr:

How to identify the CAN bus status as bus off or normal state without receiving data ?  Through reading register CAN_ESR1[BOFFINT]?

BR,

shingo

0 Kudos
Reply