no fee and fls modules in RTD of s32k3x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

no fee and fls modules in RTD of s32k3x

跳至解决方案
957 次查看
LewisThin
Contributor III

there are no some module in RTDs

LewisThin_0-1712633350188.png

I have installed RTD 4.0.0 P16  and 4.0.0 P20, but there is no fls and fee moudes in the EB config page when i choose ASAR4.7 version

LewisThin_1-1712633476099.png

 

but when i choose ASAR 4.4,  the version of other modules is V2.0.0, which are not the modules in this RTD

LewisThin_2-1712633616525.png

so, i can not use the RTD to create a project with RTD version v4.0.0

 

0 项奖励
回复
1 解答
801 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Unfortunately, all S32K3 v4.0.0 releases only support ASR R21-11 in whole or in part (ASR 4.4 is supported on Memory drivers in a few releases).
That means there won't be a release package that matches your requirements. Even older release package - v3.0.0 has started supporting ASR R21-11 instead of ASR 4.4.
So I think you should use v4.0.0 P20 with a mixed configuration between ASR R21-11 and ASR 4.4.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
910 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

This is the Significant Change between AUTOSAR 4.4 and 4.7:

AUTOSAR 4.4 VS R21-11(4.7) Significant Change.pngAUTOSAR 4.4 VS R21-11(4.7) Significant Change2.png

Please use those new modules when using AUTOSAR 4.7 version.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
889 次查看
LewisThin
Contributor III

Thanks for your kind reply. I must appologyze for the statements of my question.

my question is that

when i choose ASAR4.4, the version of fls and fee is V4.0.0, but the version of other modules,such as canif, adc is not V4.0.0,so I can not create a ASAR4.4 project with all needed modules that with version 4.0.0

0 项奖励
回复
802 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Unfortunately, all S32K3 v4.0.0 releases only support ASR R21-11 in whole or in part (ASR 4.4 is supported on Memory drivers in a few releases).
That means there won't be a release package that matches your requirements. Even older release package - v3.0.0 has started supporting ASR R21-11 instead of ASR 4.4.
So I think you should use v4.0.0 P20 with a mixed configuration between ASR R21-11 and ASR 4.4.

0 项奖励
回复
830 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

canif, adc... are not of S32K3_S32M27x Real-Time Drivers ASR 4.4 Version 4.0.0 P20. I guess you have installed more than S32K3 P16 and S32K3 P20.

Look on the Release Notes of P20:

Robin_Shen_0-1714360236958.png

So, it means P20 provide Fee, Fls, Eep on asr 4.4.0 and the rest on asr 21-11

0 项奖励
回复