What is the time for the S32K1's power supply to rise to the RESET pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the time for the S32K1's power supply to rise to the RESET pin?

1,053 Views
jingfang
Contributor IV

What is the time for the S32K1's power supply to rise to the RESET pin?

0 Kudos
Reply
4 Replies

1,031 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @jingfang,

It depends on the power supply ramp rate:

danielmartynek_3-1690874790095.png

Once VDDX reaches 2.7V, which is the Low Voltage Reset Deassert threashold, the MCU leaves the system reset.

danielmartynek_2-1690874763315.png

In the datasheet, you can find these specifications:

 

danielmartynek_0-1690874384671.png

 

Regards,

Daniel

0 Kudos
Reply

767 Views
Nibesh
Contributor III

Hello @danielmartynek 
Thank you very much for your clarification. I have understood it.
But if can you tell me roughly, how much time it will take to jump to Application, when we normally Reset the MCU.
Actually I am achieving 4.22ms, for your kind reference I have attached Logic Analyzer image.
I hope you will correlate my doubts.

One more Doubts @danielmartynek  

Will you clarify my one Doubts, on the Datasheet the Flash Timing Specification for (Program Section
execution time) (1KB flash)  is 5ms.
So when the Micro-controller is Powered, does it is taking 5ms to jump into the Application Program?
For you kind reference I took snap from the datasheet. I hope you will check Flash Timing Specifications Image for it.

I hope to hear from you Soon

BR 
Nibesh

0 Kudos
Reply

758 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Nibesh,

Can you put it into a new thread?

This is not related to the subject of this thread.

 

Regards,

Daniel

0 Kudos
Reply

755 Views
Nibesh
Contributor III
Yeah Sure will keep on new thread Daniel.

Thank you.
0 Kudos
Reply