The receiving interrupt of S32K344 can cannot be triggered

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The receiving interrupt of S32K344 can cannot be triggered

跳至解决方案
233 次查看
SCoder41
Contributor I

Why is the Rx FIFO Transfer Type option invalid in my S32DS3.5 (RTD3.0.0) project, but it is valid and optional in the S32DS3.4 (RTD2.0.0) project downloaded from the NXP community1.png2.png

0 项奖励
回复
1 解答
167 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I see transfer type can be selected, but here an error is different. 
When Legacy FIFO is enabled then CAN FD cannot be used.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
3 回复数
219 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you have CAN FD enabled then only Enhanced RXFIFO can be used. This is only available on FlexCAN0, so that's why option for transfer type is greyed.
If you disable CAN FD and enable Legacy RxFIFO then you will have this option accessible.

BR, Petr 

0 项奖励
回复
172 次查看
SCoder41
Contributor I

But,my Flexcan_0 can not do it too.问题1.png 

0 项奖励
回复
168 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I see transfer type can be selected, but here an error is different. 
When Legacy FIFO is enabled then CAN FD cannot be used.

BR, Petr

0 项奖励
回复