The receiving interrupt of S32K344 can cannot be triggered

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The receiving interrupt of S32K344 can cannot be triggered

ソリューションへジャンプ
188件の閲覧回数
SCoder41
Contributor I

Why is the Rx FIFO Transfer Type option invalid in my S32DS3.5 (RTD3.0.0) project, but it is valid and optional in the S32DS3.4 (RTD2.0.0) project downloaded from the NXP community1.png2.png

0 件の賞賛
返信
1 解決策
122件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I see transfer type can be selected, but here an error is different. 
When Legacy FIFO is enabled then CAN FD cannot be used.

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
174件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you have CAN FD enabled then only Enhanced RXFIFO can be used. This is only available on FlexCAN0, so that's why option for transfer type is greyed.
If you disable CAN FD and enable Legacy RxFIFO then you will have this option accessible.

BR, Petr 

0 件の賞賛
返信
127件の閲覧回数
SCoder41
Contributor I

But,my Flexcan_0 can not do it too.问题1.png 

0 件の賞賛
返信
123件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I see transfer type can be selected, but here an error is different. 
When Legacy FIFO is enabled then CAN FD cannot be used.

BR, Petr

0 件の賞賛
返信