The receiving interrupt of S32K344 can cannot be triggered

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The receiving interrupt of S32K344 can cannot be triggered

Jump to solution
185 Views
SCoder41
Contributor I

Why is the Rx FIFO Transfer Type option invalid in my S32DS3.5 (RTD3.0.0) project, but it is valid and optional in the S32DS3.4 (RTD2.0.0) project downloaded from the NXP community1.png2.png

0 Kudos
Reply
1 Solution
119 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I see transfer type can be selected, but here an error is different. 
When Legacy FIFO is enabled then CAN FD cannot be used.

BR, Petr

View solution in original post

0 Kudos
Reply
3 Replies
171 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you have CAN FD enabled then only Enhanced RXFIFO can be used. This is only available on FlexCAN0, so that's why option for transfer type is greyed.
If you disable CAN FD and enable Legacy RxFIFO then you will have this option accessible.

BR, Petr 

0 Kudos
Reply
124 Views
SCoder41
Contributor I

But,my Flexcan_0 can not do it too.问题1.png 

0 Kudos
Reply
120 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I see transfer type can be selected, but here an error is different. 
When Legacy FIFO is enabled then CAN FD cannot be used.

BR, Petr

0 Kudos
Reply