The difference between FX32K and FS32K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The difference between FX32K and FS32K

2,944 Views
OliverTian
NXP Employee
NXP Employee

Hello, 

     If the full P/N of FX32K and FS32K have the only difference on 'X' and 'S', these two chips could be pin-2-pin compatible on hardware. The only difference for SW should be taken care on the default value of SDID register. Detail of SDID could be checked on S32K1xx reference manual

    FX32K and FS32K use the same data sheet and reference manual.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/s32k-automotive-mc...

Cheers!

Oliver

Tags (2)
0 Kudos
Reply
2 Replies

1,004 Views
KLMan
NXP Employee
NXP Employee

if the only differnet is X and S, SDID should be exactly same since they are identical part, am I correct?

0 Kudos
Reply

1,827 Views
LucasPirola
Contributor I

Inside the S32K-DS.pdf is attached an excel files with the Orderable Part Numbers for S32K microcontrollers, and as of Rev. 10, this file does NOT include any part number starting with FX32K.  This led to confusion and time consuming activities in my team. This information now seems stable enough to be added to the list and avoid further confusion.

0 Kudos
Reply