Siul2_Port_Ip_Init & Hi-Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Siul2_Port_Ip_Init & Hi-Z

ソリューションへジャンプ
2,482件の閲覧回数
jetty_1012
Contributor II

Hi,

I have configured some ports on S32 DS.

And I know this API Siul2_Port_Ip_Init is used to initialize the ports.

My questioin is, if the ports that I configured on S32 DS are not initialized, are they Hi-Z?

 

Thanks,

Jetty

0 件の賞賛
返信
1 解決策
2,460件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jetty_1012 

When you don't configure a pin, it maintains the same state it has after a power-up. 

Please refer to section 4.5 (Pin States) of the S32K3xx Reference Manual, Rev. 6.

 

B.R.

VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,461件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jetty_1012 

When you don't configure a pin, it maintains the same state it has after a power-up. 

Please refer to section 4.5 (Pin States) of the S32K3xx Reference Manual, Rev. 6.

 

B.R.

VaneB

0 件の賞賛
返信