S32K3xx Flash minimum P/E cycles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3xx Flash minimum P/E cycles

Jump to solution
962 Views
damy
Contributor I

From the S32K3xx datasheet (Rev. 5.1 10/2022) Chapter 9.3, Table 28:

The minimum "Number of program/erase cycles per block for 256 KB and 512 KB blocks using Sector Erase." is stated as 100,000 P/E cycles.

However, it is a bit unclear from the description if every sector P/E cycle counts towards the P/E cycle of the block. So, my question is, is the minimum 100,000 P/E cycles per sector? Or is the minimum 100,000 P/E cycles the sum of all sectors in a block?

Thanks in advance.

Damy

0 Kudos
Reply
1 Solution
952 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I would even simplify it - P/E is basically erase cycle for smaller unit you can erase, what’s sector in this case.

Within flash endurance specification it is only important which block this particular sector belongs to. Every sector of 256KB/512KB block is capable to withstand 100,000 erase cycles.

View solution in original post

0 Kudos
Reply
1 Reply
953 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I would even simplify it - P/E is basically erase cycle for smaller unit you can erase, what’s sector in this case.

Within flash endurance specification it is only important which block this particular sector belongs to. Every sector of 256KB/512KB block is capable to withstand 100,000 erase cycles.

0 Kudos
Reply