S32K3X4EVBQ257ND embedded demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3X4EVBQ257ND embedded demo

Jump to solution
1,080 Views
radudrosescu
Contributor III

Hello,

S32K3X4EVBQ257ND embedded board comes with a demo program included. It should be accessible as a project or source, in order to be able to bring the board to its original condition after testing. I was unable to identify this demo between the S32DS Project from Example. Can be downloaded this demo? I do not consider the possibility of saving it before any test as object file with the help of the debugger.

Thanks!

Radu

Tags (1)
0 Kudos
Reply
1 Solution
1,034 Views
radudrosescu
Contributor III

O.K! This app is no big deal, I'm surprised to keep it top secret. The problem is that in order to save the source (binary code) and then to reflash demo you need an additional Multilink Fx and P&E PROGACM-Flashprogrammer, ie. 600 USD + VAT. Notice to those who purchase this evaluating board.

Regards,

Radu

View solution in original post

0 Kudos
Reply
3 Replies
1,035 Views
radudrosescu
Contributor III

O.K! This app is no big deal, I'm surprised to keep it top secret. The problem is that in order to save the source (binary code) and then to reflash demo you need an additional Multilink Fx and P&E PROGACM-Flashprogrammer, ie. 600 USD + VAT. Notice to those who purchase this evaluating board.

Regards,

Radu

0 Kudos
Reply
1,059 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Radu,

let me ask if the source code is available.

Regards,

Lukas

0 Kudos
Reply
1,042 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

I'm sorry, it's not possible to provide the source code.

Regards,

Lukas

0 Kudos
Reply