S32K3X4EVBQ257ND embedded demo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3X4EVBQ257ND embedded demo

跳至解决方案
768 次查看
radudrosescu
Contributor III

Hello,

S32K3X4EVBQ257ND embedded board comes with a demo program included. It should be accessible as a project or source, in order to be able to bring the board to its original condition after testing. I was unable to identify this demo between the S32DS Project from Example. Can be downloaded this demo? I do not consider the possibility of saving it before any test as object file with the help of the debugger.

Thanks!

Radu

标记 (1)
0 项奖励
1 解答
722 次查看
radudrosescu
Contributor III

O.K! This app is no big deal, I'm surprised to keep it top secret. The problem is that in order to save the source (binary code) and then to reflash demo you need an additional Multilink Fx and P&E PROGACM-Flashprogrammer, ie. 600 USD + VAT. Notice to those who purchase this evaluating board.

Regards,

Radu

在原帖中查看解决方案

0 项奖励
3 回复数
723 次查看
radudrosescu
Contributor III

O.K! This app is no big deal, I'm surprised to keep it top secret. The problem is that in order to save the source (binary code) and then to reflash demo you need an additional Multilink Fx and P&E PROGACM-Flashprogrammer, ie. 600 USD + VAT. Notice to those who purchase this evaluating board.

Regards,

Radu

0 项奖励
747 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Radu,

let me ask if the source code is available.

Regards,

Lukas

0 项奖励
730 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

I'm sorry, it's not possible to provide the source code.

Regards,

Lukas

0 项奖励