S32K3X4EVBQ257ND embedded demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3X4EVBQ257ND embedded demo

ソリューションへジャンプ
787件の閲覧回数
radudrosescu
Contributor III

Hello,

S32K3X4EVBQ257ND embedded board comes with a demo program included. It should be accessible as a project or source, in order to be able to bring the board to its original condition after testing. I was unable to identify this demo between the S32DS Project from Example. Can be downloaded this demo? I do not consider the possibility of saving it before any test as object file with the help of the debugger.

Thanks!

Radu

タグ(1)
0 件の賞賛
1 解決策
741件の閲覧回数
radudrosescu
Contributor III

O.K! This app is no big deal, I'm surprised to keep it top secret. The problem is that in order to save the source (binary code) and then to reflash demo you need an additional Multilink Fx and P&E PROGACM-Flashprogrammer, ie. 600 USD + VAT. Notice to those who purchase this evaluating board.

Regards,

Radu

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
742件の閲覧回数
radudrosescu
Contributor III

O.K! This app is no big deal, I'm surprised to keep it top secret. The problem is that in order to save the source (binary code) and then to reflash demo you need an additional Multilink Fx and P&E PROGACM-Flashprogrammer, ie. 600 USD + VAT. Notice to those who purchase this evaluating board.

Regards,

Radu

0 件の賞賛
766件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Radu,

let me ask if the source code is available.

Regards,

Lukas

0 件の賞賛
749件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

I'm sorry, it's not possible to provide the source code.

Regards,

Lukas

0 件の賞賛