Hello.
I have problem with use S32K312, ADC0_S9
I read below articles.
https://community.nxp.com/t5/S32K/S32K344-ADC-HAS-ADC-INTERLEAVE-problem/m-p/1548855
https://community.nxp.com/t5/S32K/S32K3-ADC-Channcal-configure-problem/td-p/1527680
My RTD version is 2.0.1 (Released 7, July, 2022).
Which RTD version fixed that problem?
Best Regards
已解决! 转到解答。
Hi
As I know this bug should be fixed in RTD_4.7_S32K3XX_3.0.0_CD04. But I did not install this version. I have install a new version S32K3_M27X Real-Time Drivers Version 3.0.0 P07. I can see that Siul2_Port_Ip_WriteDCMConfiguration has changed.
By the way, those S32K3 RTD 3.0.0 should be installed in S32DS v3.5. That means you need to install S32DS v3.5 instead of updating RTD in v3.4.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
As I know this bug should be fixed in RTD_4.7_S32K3XX_3.0.0_CD04. But I did not install this version. I have install a new version S32K3_M27X Real-Time Drivers Version 3.0.0 P07. I can see that Siul2_Port_Ip_WriteDCMConfiguration has changed.
By the way, those S32K3 RTD 3.0.0 should be installed in S32DS v3.5. That means you need to install S32DS v3.5 instead of updating RTD in v3.4.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------