How can I connect the OM14500 to the S32K148-Q176 Evaluation Board without using the J16 connector, is direct soldering from the pins of the OM14550 the only way?
解決済! 解決策の投稿を見る。
Hi @OTSL-J
if you want to use TJA1101 PHY with S32K148, use this board instead of OM14500:
This is a plug&play solution.
I can't see simple way how to connect OM14500 to the S32K148EVB.
Regards,
Lukas
If I want to change from RMII interface to MII interface, is it provided in the software provided by NXP S32K148 EVB?
Yes, our SW provides an option to switch between MII or RMII. For example:
But if you want to use mentioned board ADTJA1101-RMII, there's no option to use MII. The board is designed to use RMII only.
Regards,
Lukas
Thank you.
Good comment.