S32K148-Q176 Evaluation Board+OM14500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148-Q176 Evaluation Board+OM14500

Jump to solution
829 Views
OTSL-J
Contributor II

How can I connect the OM14500 to the S32K148-Q176 Evaluation Board without using the J16 connector, is direct soldering from the pins of the OM14550 the only way?

0 Kudos
Reply
1 Solution
765 Views
OTSL-J
Contributor II

Thank you.

Good comment.

View solution in original post

0 Kudos
Reply
4 Replies
813 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @OTSL-J 

if you want to use TJA1101 PHY with S32K148, use this board instead of OM14500:

https://www.nxp.com/products/interfaces/ethernet-/automotive-ethernet-phys/tja1101-automotive-ethern...

This is a plug&play solution.

I can't see simple way how to connect OM14500 to the S32K148EVB.

Regards,

Lukas

0 Kudos
Reply
791 Views
OTSL-J
Contributor II

If I want to change from RMII interface to MII interface, is it provided in the software provided by NXP S32K148 EVB?

0 Kudos
Reply
781 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, our SW provides an option to switch between MII or RMII. For example:

lukaszadrapa_0-1698142017582.png

But if you want to use mentioned board ADTJA1101-RMII, there's no option to use MII. The board is designed to use RMII only.

Regards,

Lukas

 

0 Kudos
Reply
766 Views
OTSL-J
Contributor II

Thank you.

Good comment.

0 Kudos
Reply