I want to operate the example of s32k144w.
TX for CAN0 is set to PTE5 RX is set to PTE4
Example uses buttons and LEDs, but I want to get rid of them all.
I want CAN signal voltage output from PTE5 and 4
Currently, I only modified g_pin_mux_InitConfigArr0 and flexcanInitConfig0.
I tried changing and erasing everything, but it didn't work.
Even the buttons and the LED codes..
If the RX signal allows the ID to be 0x300 to receive the signal, I will add it on my own after that.
I really hope you can help me. I've been walking in place for three days.
I have checked your code,please refer to this article to modified your demo code.
your clock setting is too slow
https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-FlexCAN-Mask-Setting-Demo/ta-p/1519753
this demo using interrupt method to receive CAN Frame, you can refer this demo to create your project.