Hi
I am using the UART using the example code from COOK BOOK below.
I would like to change the UART speed from 9600 to 115200, but I do not know how to modify it in the code below.
Let me know how to use the modified code and USRT easily.
/*******************************************************************************************************/
void LPUART1_init(void) /* Init. summary: 9600 baud, 1 stop bit, 8 bit format, no parity */
{
PCC->PCCn[PCC_LPUART1_INDEX] &= ~PCC_PCCn_CGC_MASK; /* Ensure clk disabled for config */
PCC->PCCn[PCC_LPUART1_INDEX] |= PCC_PCCn_PCS(0b001) /* Clock Src= 1 (SOSCDIV2_CLK) */
| PCC_PCCn_CGC_MASK; /* Enable clock for LPUART1 regs */
LPUART1->BAUD = 0x0F000034; /* Initialize for 9600 baud, 1 stop: */
/* SBR=52 (0x34): baud divisor = 8M/9600/16 = ~52 */
/* OSR=15: Over sampling ratio = 15+1=16 */
/* SBNS=0: One stop bit */
/* BOTHEDGE=0: receiver samples only on rising edge */
/* M10=0: Rx and Tx use 7 to 9 bit data characters */
/* RESYNCDIS=0: Resync during rec'd data word supported */
/* LBKDIE, RXEDGIE=0: interrupts disable */
/* TDMAE, RDMAE, TDMAE=0: DMA requests disabled */
/* MAEN1, MAEN2, MATCFG=0: Match disabled */
LPUART1->CTRL=0x000C0000; /* Enable transmitter & receiver, no parity, 8 bit char: */
/* RE=1: Receiver enabled */
/* TE=1: Transmitter enabled */
/* PE,PT=0: No hw parity generation or checking */
/* M7,M,R8T9,R9T8=0: 8-bit data characters*/
/* DOZEEN=0: LPUART enabled in Doze mode */
/* ORIE,NEIE,FEIE,PEIE,TIE,TCIE,RIE,ILIE,MA1IE,MA2IE=0: no IRQ*/
/* TxDIR=0: TxD pin is input if in single-wire mode */
/* TXINV=0: TRansmit data not inverted */
/* RWU,WAKE=0: normal operation; rcvr not in statndby */
/* IDLCFG=0: one idle character */
/* ILT=0: Idle char bit count starts after start bit */
/* SBK=0: Normal transmitter operation - no break char */
/* LOOPS,RSRC=0: no loop back */
}
已解决! 转到解答。
Hi KWAK D.Y,
I changed the code, for example, for LPUART source clock 40MHz. I assume, your oscillator and clocks settings are the same as in the LPUART example and SPLLDIV2_CLK is set to 40MHz.
Our aim is to find such a ratio to make the error as close as possible to 0. In this case is the error -0.22%
PCC->PCCn[PCC_LPUART1_INDEX] &= ~PCC_PCCn_CGC_MASK; // Ensure clk disabled for config
PCC->PCCn[PCC_LPUART1_INDEX] |= PCC_PCCn_PCS(0b110) // Source clock for LPUART1 is SPLLDIV2_CLK
| PCC_PCCn_CGC_MASK; // Enable clock for LPUART1 regs
LPUART1->BAUD = 0x1C00000C; /* Initialize for 115200 baud, 1 stop: */
/* SBR=12 (0xC):
baud divisor = Source clock/ Baud rate/ OSR+1 = 40000000/115200/29 =11.97 => ~12*/
/* OSR=28: Over sampling ratio = 28+1=29 */
/* SBNS=0: One stop bit */
/* BOTHEDGE=0: receiver samples on the rising edge*/
/* M10=0: Rx and Tx use 7 to 9 bit data characters */
/* RESYNCDIS=0: Resync during rec'd data word supported */
/* LBKDIE, RXEDGIE=0: interrupts disable */
/* TDMAE, RDMAE, TDMAE=0: DMA requests disabled */
/* MAEN1, MAEN2, MATCFG=0: Match disabled */
For better understanding I recommend you to see chapter 51.4.1 Baud rate generation in the reference manual.
I hope it helps you.
Best regards,
Diana
Hi KWAK D.Y,
I changed the code, for example, for LPUART source clock 40MHz. I assume, your oscillator and clocks settings are the same as in the LPUART example and SPLLDIV2_CLK is set to 40MHz.
Our aim is to find such a ratio to make the error as close as possible to 0. In this case is the error -0.22%
PCC->PCCn[PCC_LPUART1_INDEX] &= ~PCC_PCCn_CGC_MASK; // Ensure clk disabled for config
PCC->PCCn[PCC_LPUART1_INDEX] |= PCC_PCCn_PCS(0b110) // Source clock for LPUART1 is SPLLDIV2_CLK
| PCC_PCCn_CGC_MASK; // Enable clock for LPUART1 regs
LPUART1->BAUD = 0x1C00000C; /* Initialize for 115200 baud, 1 stop: */
/* SBR=12 (0xC):
baud divisor = Source clock/ Baud rate/ OSR+1 = 40000000/115200/29 =11.97 => ~12*/
/* OSR=28: Over sampling ratio = 28+1=29 */
/* SBNS=0: One stop bit */
/* BOTHEDGE=0: receiver samples on the rising edge*/
/* M10=0: Rx and Tx use 7 to 9 bit data characters */
/* RESYNCDIS=0: Resync during rec'd data word supported */
/* LBKDIE, RXEDGIE=0: interrupts disable */
/* TDMAE, RDMAE, TDMAE=0: DMA requests disabled */
/* MAEN1, MAEN2, MATCFG=0: Match disabled */
For better understanding I recommend you to see chapter 51.4.1 Baud rate generation in the reference manual.
I hope it helps you.
Best regards,
Diana