Hello ,
In my project,I found that:
when I operate 'erase flash' or 'write flash' , syetem will reset,
therefore,I add sentence in main() as below(founded in cookbook) and system working normally:
LMEM->PCCCR = LMEM_PCCCR_INVW0(1) | LMEM_PCCCR_INVW1(1) | LMEM_PCCCR_GO(1) | LMEM_PCCCR_ENCACHE(1);
but this sentence maybe have an effect on driver - interrupt(such as SPI,UART,etc.)
for example:
Before: I set UART(460800,int-priority-5)/SPI0(10M,int-priority-5)/SPI1(10M,int-priority-5) and system working normally
After:I have to set UART(460800,int-priority-5)/SPI0(1M,int-priority-7) SPI0(1M,int-priority-7)
If I don't set like After , interrupt maybe working weirdly(eg. data missing sometimes) ,I have to modify priority and cut down SPI-bautrate to guarantee data-completeness,
Dose anyone know this?
If anyone has any idea,please share with me ,thanks very very much.
Hello langweihua1643@163.com,
Regarding the reset, you probably launch the PFlash FTFC commands from the PFlash partition (there is only one PFlash partition on S32K144).
You need to execute the code that launches the FTFC commands (clear CCIF, wait until CCIF = 1) from a different flash partition (DFlash on S32K144) or SRAM.
Do you invalidate the Cache after the FTTC programming/erasing?
Regards,
Daniel