[S32K144] FlexIO - config two groups of uart

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32K144] FlexIO - config two groups of uart

1,257件の閲覧回数
呈源黄
Contributor I

Hi, can I config two groups of UART by FlexIO?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,119件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Yes, you can configure 2x UART by FlexIO.

Note:

If we check chapter "52.1.1 FlexIO Configuration" in the RM rev 9. we can see that there are 4x Timer, 4x Shifter, and 8x Pin.

For the one UART receive we need 1x shifter and 1x timer and for the transmit, we need 1x shifter and 1x timer.

So, we can configure max 2x UART by FlexIO.

I hope it helps.

Best Regards,

Diana

0 件の賞賛
返信

1,063件の閲覧回数
Simin
Contributor II

Hi,

        If I want using FLEXIO shifter working in ‘Match store mode’ or 'Match continuous mode'

        Could you help me how to configure this function,and the applicaton case when we use

these two mode

Best regard,

Simin

0 件の賞賛
返信