We use S32K142W, and SDK is 4.0.3.
We want use internal simulation eeprom, referred to example <flash_partitioning_s32k142w>.
It looks like the initialization is fine.
But when access with eeprom addr, like 0x14000001, will jump to DefaultISR.
Debug as follow picture.
Attached is my project file.
解決済! 解決策の投稿を見る。
Hi @346500452,
I see now you have the S32K142W part.
There is the FTFM module that supports 32bit aligned writes only.
Unlike the FTFC module on other S32K14x parts:
Regards,
Daniel
Hi @346500452,
I see now you have the S32K142W part.
There is the FTFM module that supports 32bit aligned writes only.
Unlike the FTFC module on other S32K14x parts:
Regards,
Daniel
Hi @346500452,
What kind if fault exception do you get there?
Can you implement the HardFault_Handler() and read the CSFR register?
https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447
BR, Daniel
Hi, @danielmartynek
I change address to access, like 0x14000000 or 0x14000004 or (0x1400000 + 4*n).
And it works ok.