We use S32K142W, and SDK is 4.0.3.
We want use internal simulation eeprom, referred to example <flash_partitioning_s32k142w>.
It looks like the initialization is fine.
But when access with eeprom addr, like 0x14000001, will jump to DefaultISR.
Debug as follow picture.
Attached is my project file.
Solved! Go to Solution.
Hi @346500452,
I see now you have the S32K142W part.
There is the FTFM module that supports 32bit aligned writes only.
Unlike the FTFC module on other S32K14x parts:
Regards,
Daniel
Hi @346500452,
I see now you have the S32K142W part.
There is the FTFM module that supports 32bit aligned writes only.
Unlike the FTFC module on other S32K14x parts:
Regards,
Daniel
Hi @346500452,
What kind if fault exception do you get there?
Can you implement the HardFault_Handler() and read the CSFR register?
https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447
BR, Daniel
Hi, @danielmartynek
I change address to access, like 0x14000000 or 0x14000004 or (0x1400000 + 4*n).
And it works ok.