[S32K11x] Does Clamp diodes exist on each pin for S32K11x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[S32K11x] Does Clamp diodes exist on each pin for S32K11x

跳至解决方案
507 次查看
GavinLi1
Contributor II

Hello Experts,

I just want to clarify that does Clamp diodes exist on each pin for S32K11x as the following picture show?

If yes, where can I can such information from RM or DS?

If no full cover each pin, which pins have the clamp diodes?

GavinLi1_0-1719926990960.png

Thanks,

Gavin

0 项奖励
回复
1 解答
441 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

Yes, all IOs are internally clamped to VDD and VSS. It is specified by the Injection current +- 3mA per a single pin and the ESD handling ratings. 

Julin_AragnM_2-1720126268720.png

Best regards,
Julián

在原帖中查看解决方案

0 项奖励
回复
4 回复数
485 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

All pins implement protection diodes that protect against electrostatic discharge (ESD). These internal ESD diodes of the microcontroller are designed just for short discharge pulses only, and these do not sustain a constant current over time.

You can find the ESD and latch-up protection characteristics in chapter 4.8 from the S32K1xx's Data Sheet.

Best regards,
Julián

0 项奖励
回复
467 次查看
GavinLi1
Contributor II

Hi Julián,
Thanks for your quick reply.

I want to further confirm that the protection diode does real exist not  the equivalent diode or parasitic diode, right?

GavinLi1_0-1720071431280.png

Thanks in advance!

Gavin

0 项奖励
回复
442 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

Yes, all IOs are internally clamped to VDD and VSS. It is specified by the Injection current +- 3mA per a single pin and the ESD handling ratings. 

Julin_AragnM_2-1720126268720.png

Best regards,
Julián

0 项奖励
回复
419 次查看
GavinLi1
Contributor II
Hi Julián,
Thanks your comfirm.

Regards,
Gavin
0 项奖励
回复