[S32K11x] Does Clamp diodes exist on each pin for S32K11x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32K11x] Does Clamp diodes exist on each pin for S32K11x

Jump to solution
506 Views
GavinLi1
Contributor II

Hello Experts,

I just want to clarify that does Clamp diodes exist on each pin for S32K11x as the following picture show?

If yes, where can I can such information from RM or DS?

If no full cover each pin, which pins have the clamp diodes?

GavinLi1_0-1719926990960.png

Thanks,

Gavin

0 Kudos
Reply
1 Solution
440 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

Yes, all IOs are internally clamped to VDD and VSS. It is specified by the Injection current +- 3mA per a single pin and the ESD handling ratings. 

Julin_AragnM_2-1720126268720.png

Best regards,
Julián

View solution in original post

0 Kudos
Reply
4 Replies
484 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

All pins implement protection diodes that protect against electrostatic discharge (ESD). These internal ESD diodes of the microcontroller are designed just for short discharge pulses only, and these do not sustain a constant current over time.

You can find the ESD and latch-up protection characteristics in chapter 4.8 from the S32K1xx's Data Sheet.

Best regards,
Julián

0 Kudos
Reply
466 Views
GavinLi1
Contributor II

Hi Julián,
Thanks for your quick reply.

I want to further confirm that the protection diode does real exist not  the equivalent diode or parasitic diode, right?

GavinLi1_0-1720071431280.png

Thanks in advance!

Gavin

0 Kudos
Reply
441 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

Yes, all IOs are internally clamped to VDD and VSS. It is specified by the Injection current +- 3mA per a single pin and the ESD handling ratings. 

Julin_AragnM_2-1720126268720.png

Best regards,
Julián

0 Kudos
Reply
418 Views
GavinLi1
Contributor II
Hi Julián,
Thanks your comfirm.

Regards,
Gavin
0 Kudos
Reply