[S32K11x] Does Clamp diodes exist on each pin for S32K11x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32K11x] Does Clamp diodes exist on each pin for S32K11x

ソリューションへジャンプ
246件の閲覧回数
GavinLi1
Contributor II

Hello Experts,

I just want to clarify that does Clamp diodes exist on each pin for S32K11x as the following picture show?

If yes, where can I can such information from RM or DS?

If no full cover each pin, which pins have the clamp diodes?

GavinLi1_0-1719926990960.png

Thanks,

Gavin

0 件の賞賛
返信
1 解決策
180件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

Yes, all IOs are internally clamped to VDD and VSS. It is specified by the Injection current +- 3mA per a single pin and the ESD handling ratings. 

Julin_AragnM_2-1720126268720.png

Best regards,
Julián

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
224件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

All pins implement protection diodes that protect against electrostatic discharge (ESD). These internal ESD diodes of the microcontroller are designed just for short discharge pulses only, and these do not sustain a constant current over time.

You can find the ESD and latch-up protection characteristics in chapter 4.8 from the S32K1xx's Data Sheet.

Best regards,
Julián

0 件の賞賛
返信
206件の閲覧回数
GavinLi1
Contributor II

Hi Julián,
Thanks for your quick reply.

I want to further confirm that the protection diode does real exist not  the equivalent diode or parasitic diode, right?

GavinLi1_0-1720071431280.png

Thanks in advance!

Gavin

0 件の賞賛
返信
181件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @GavinLi1,

Yes, all IOs are internally clamped to VDD and VSS. It is specified by the Injection current +- 3mA per a single pin and the ESD handling ratings. 

Julin_AragnM_2-1720126268720.png

Best regards,
Julián

0 件の賞賛
返信
158件の閲覧回数
GavinLi1
Contributor II
Hi Julián,
Thanks your comfirm.

Regards,
Gavin
0 件の賞賛
返信