S32K uses PLL, can use external crystal 4M?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K uses PLL, can use external crystal 4M?

ソリューションへジャンプ
1,598件の閲覧回数
xiabin
Contributor II

I am using the S32K configuration tool, PLL use osc 4m, clock diveder = 1; Information:

warning:the result frequency must between 8m to 32m.

タグ(1)
0 件の賞賛
返信
1 解決策
1,465件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Xia bin

Not, unfortunately, SPLL reference frequency range is Min 8MHz and max 16MHz, so, you can't use it with an osc of 4M. Sorry for the inconveniences:

https://www.nxp.com/docs/en/data-sheet/S32K1XX.pdf#page=33 

Best regards

Jorge Alcala

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,466件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Xia bin

Not, unfortunately, SPLL reference frequency range is Min 8MHz and max 16MHz, so, you can't use it with an osc of 4M. Sorry for the inconveniences:

https://www.nxp.com/docs/en/data-sheet/S32K1XX.pdf#page=33 

Best regards

Jorge Alcala

0 件の賞賛
返信