hi,
i"m using the s32k142 with RUN mode and VLPS mode, through the GPIO interrupt to wake up the chip from VLPS mode, it's working fine in most of times,but there is a slight chance that can't wake up from VLPS mode,only reconnect the power can make chip normal.this situation happened in different boards and can't reproduce.
I would like to know,what situation may cause the MCU can't wake up from VLPS mode? thank you very much.
BR
已解决! 转到解答。
Hi,
Could you please make sure that PREDIV_SYS_CLK frequency / BUS_CLK frequency configuration for RUN/VLPR mode is greater than or equal to 2 before executing the transition to VLPS.
Mask Set Errata for Mask 0N33V
https://www.nxp.com/docs/en/errata/S32K142_0N33V.pdf
ERR011063
Thank you,
BR, Daniel
Hi,
Please make sure that the interrupts are not masked when the MCU enters VLPS.
You could try using the highest interrupt priority only for the interrupts that are used to wake the MCU up.
BR, Daniel
hi,
we enabled the PORTB interrupts before enters VLPS, the wake up source was connected with PTB ,the priority was highest.
and , it can wake up normally at the most of times,just 2 or 3 times dead in VLPS.
Hi,
Could you please make sure that PREDIV_SYS_CLK frequency / BUS_CLK frequency configuration for RUN/VLPR mode is greater than or equal to 2 before executing the transition to VLPS.
Mask Set Errata for Mask 0N33V
https://www.nxp.com/docs/en/errata/S32K142_0N33V.pdf
ERR011063
Thank you,
BR, Daniel
Hi Daniel,
I checked my clock configuration and maybe it's the reason.
and I was wondering whether there should be some inconsistency about the data in the example. Based on the errata, the dividers in red circles should not be the same but parameters is the same.
thank you !