S32 DS 3.5新建工程没有SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 DS 3.5新建工程没有SDK

709 Views
Vapaus
Contributor III

S32K118新建工程时没有SDK可选

Vapaus_1-1708914388534.png

 

 

0 Kudos
Reply
2 Replies

696 Views
Robin_Shen
NXP TechSupport
NXP TechSupport
Hi
It is recommended to install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4.
Or install S32K1 RTD 2.0.x with S32DS Extensions and Updates in S32DS v3.5.
Do not use S32K1 SDK 4.0.1 with S32DS v3.5. According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version.
 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

671 Views
Vapaus
Contributor III
我们是S32K118平台,MCAL版本是4.3, 上面帖子版本SDK RTM 4.0.3的,方法不通用吧
0 Kudos
Reply