I enabled the pins configuration tool in the default FlexCAN_Ip_Example_S32K344 to observe the CAN0 Tx output on the PTA7 pin in the normal mode. I was able to see the digital CAN signals on the oscilloscope.
But when I changed the output port from PTA7 to PTB1, I couldn't see any signals on the oscilloscope.
I also tried changing CAN0 to CAN1, but still I can only see signals from the PTA7 port.
Is there any reason why can't I observe CAN signals from any ports other than PTA7 becuase in schematics both PTA7 and PTB1 can have CAN0_Tx signal.
I am using S32K3X4EVB-T172 board have attached the project.
解決済! 解決策の投稿を見る。
Hi @sagar991,
Sorry for the misunderstanding, only pins PTA6 & PTA7 are connected to the PHY on board:
If you need to use another pin for transmission, they need to be rerouted.
Best regards,
Julián
Hi @sagar991,
Are you testing this with two S32K344 boards?
In order to see the signals for the transmissions, you will need another CAN node in the bus (either another MCU or CAN analyzer).
Best regards,
Julián.
Hi @sagar991,
Sorry for the misunderstanding, only pins PTA6 & PTA7 are connected to the PHY on board:
If you need to use another pin for transmission, they need to be rerouted.
Best regards,
Julián