PWM GetDutyCycle gives inconsistent period readings on a constant duty PWM (S32K358, RTD4.0.0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PWM GetDutyCycle gives inconsistent period readings on a constant duty PWM (S32K358, RTD4.0.0)

969 次查看
RChatterjee
Contributor III

I am getting different period values when I use Emios_Icu_Ip_GetDutyCycleValues(). However, the active time stays consistent. How do I remove this inconsistency?

PFA

标记 (2)
0 项奖励
回复
1 回复

928 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Just a quick reply.

Please refer to the S32K344_Example_Emios_Icu_IPWM_measurement_DS34_RTD_100_v2

Or check the returned value of Emios_Icu_Ip_GetInputState before call Emios_Icu_Ip_GetDutyCycleValues.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复