Hi NXP team,
I am using S32K144 controller in our project.
I used the meset() with linker script global variables.
memset(&__FSLCODE_SECTION_START, 0x00, __FSLCODE_SECTION_END - __FSLCODE_SECTION_START);
but that FSL code segment (section) is not set to zero.
find the attached document for more information on memeset() problem.
Regarding the watchdog timer :
I used the code given in the reference manual for watchdog configuration
DISABLE_INTERRUPTS(); // disable global interrupt
WDOG->CNT = 0xD928C520; //unlock watchdog
while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0); //wait until registers are unlocked
WDOG->TOVAL = 256; //set timeout value
WDOG->CS = WDOG_CS_EN(1) | WDOG_CS_CLK(1) | WDOG_CS_INT(0) |
WDOG_CS_WIN(0) | WDOG_CS_UPDATE(0);
while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0); //wait until new configuration takes effect
ENABLE_INTERRUPTS(); //enable global interrupt
if(WDOG->CNT >= 125)
{
DISABLE_INTERRUPTS(); // disable global interrupt
WDOG->CNT = 0xB480A602; // refresh watchdog
ENABLE_INTERRUPTS(); //
}
in the above code , control not come out of the while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0);
Kindly help in this.
Regards,
Ambarish
Hi Raju,
//if(timeout_s > 127) return PUBLIC_STATUS_ERROR;
INT_SYS_DisableIRQGlobal();
WDOG->CNT = 0xD928C520; // Unlock WDOG
while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0);
WDOG->TOVAL =timeout_ms;//128 * timeout_s; // Timeout in max = 65535 * (1 / 1 kHz) = 65535ms
//WDOG->CS = WDOG_CS_EN(1)|WDOG_CS_CLK(1)|WDOG_CS_INT(1)|WDOG_CS_WIN(0)|WDOG_CS_UPDATE(0);
WDOG->CS = WDOG_CS_EN(1) | WDOG_CS_CLK(1) | WDOG_CS_INT(0) | WDOG_CS_WIN(0) | WDOG_CS_UPDATE(0) | WDOG_CS_DBG(1);
while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0);
INT_SYS_EnableIRQGlobal();
It's stuck here
while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0);
Hi Wang,
If you are trying to update/ reconfigure the watchdog after initial watchdog configuration like initial disable watchdog function or something
I suggest you use WDOG_CS_UPDATE(1) in your initial watchdog configuration.
Raju
Hi,
Regarding the watchdog, the code works on my side with both masksets (0N47T, 0N57U) as expected.
There is a restriction that the reconfiguration must be done within 128 bus cycles.
So you cannot step the code.
Regards,
Daniel
@Hello Daniel,
Thank you for your support.
could you please share your complete tested source code.
I tried with toggling the LED while refreshing the watchdog , but LED is not toggling.
directly flashed the code and checked.
EVAL board has PS32K144HFVLL 0N77P controller chip.
PCC-> PCCn[PCC_PORTD_INDEX] = PCC_PCCn_CGC_MASK; /* Enable clock for PORT D */
PTD->PDDR |= 1<<0; /* Port D0: Data Direction= output */
PORTD->PCR[0] = 0x00000100; /* Port D0: MUX = ALT1, GPIO (to blue LED on EVB) */ WDOG->CNT = 0xD928C520; //unlock watchdog
DISABLE_INTERRUPTS();
while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0); //wait until registers are unlocked
WDOG->TOVAL = 0x1E8480; // used the default clock configuration , not configured clock in the code //set the count to 2000000
WDOG->CS = WDOG_CS_EN(1) | WDOG_CS_CLK(1) | WDOG_CS_INT(0) |
WDOG_CS_WIN(0) | WDOG_CS_UPDATE(0);
while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0); //wait until new configuration takes effect
ENABLE_INTERRUPTS(); //enable global interrupt
while(1)
{
//PTD->PDDR = 1;
if(WDOG->CNT >= 0xF4240) //if count is equal or greater 1000000
{
DISABLE_INTERRUPTS(); // disable global interrupt
WDOG->CNT = 0xB480A602; // refresh watchdog
ENABLE_INTERRUPTS(); //
PTD->PTOR |= 1<<0;
}
}
Thanks,
Ambarish
Hello Ambarish,
The problem is in the maskset (0N77P).
Please use either 0N47T or preferably 0N57U which is the production version.
There are many differences between 0N77P and 0N47T/0N57U.
The current RM is not compatible with that maskset.
WDOG_CS[ULK] is not present on 0N77P thus it reads 0.
Regards,
Daniel
Hi Daniel,
Is there any similar issue with S32K142.
Raju
Hi Raju,
No, there is no such issue with the S32K142.
There is only one S32K142 mask 0N33V covered by the S32K1xx RM, DS.
BR, Daniel
Hi Daniel,
Thanks for the response.
I'm trying to implement the watchdog code and the code just has a while(1) loop with the below code. I expect the code will reset so I set a breakpoint at the start of the code to ensure the reset. But it still there is no reset happened.
DISABLE_INTERRUPTS();
WDOG->CNT = 0xD928C520; //unlock watchdog
while(((WDOG->CS & WDOG_CS_ULK_MASK) >> WDOG_CS_ULK_SHIFT) == 0); //wait until registers are unlocked
WDOG->TOVAL = 256; // used the default clock configuration , not configured clock in the code //set the count to 2000000
WDOG->CS = WDOG_CS_EN(1) | WDOG_CS_CLK(1) | WDOG_CS_INT(0) |
WDOG_CS_WIN(0) | WDOG_CS_UPDATE(0);
while(((WDOG->CS & WDOG_CS_RCS_MASK ) >> WDOG_CS_RCS_SHIFT) == 0); //wait until new configuration takes effect
ENABLE_INTERRUPTS(); //enable global interrupt
Kindly suggest us a solution
Raju.
Thanks Daniel. It is working now. Thanks for the support.
Raju